TX_PDOx_Event_Timer
Index.Sub |
|
||||||||||
Data Type | Unsigned16 | ||||||||||
Access | Read/Write | ||||||||||
PDO Mappable | No | ||||||||||
Unit |
milliseconds (ms) |
||||||||||
Range |
0, 65535 | ||||||||||
Default Value | 100 | ||||||||||
Store Supported | Yes | ||||||||||
Description | This is the event timer of TX_PDOx. If value equal to 0 the TX_PDOx is transmitted only when it changes. If value > 0 the TX_PDOx is transmitted every event timer milliseconds. | ||||||||||
Notes |
|